• EH 22111. Index Plungers with Push-Lock locking mechanism
    These index plungers can be locked / released with the press of a button. The push-lock function is based on the installed mechanical system, which operates on the familiar “ball pen principle.” Their design and functionality make these index plungers an excellent choice for cramped installation situations. When latched, the index plunger can be countersunk to protect it against faulty operation.

 

 

Here you will find additional information on our Index Plungers / Index Bolts​​​​​​​.